EEO#.LINES
Description
Sets how many lines are output for one revolution of the source feedback. When configured to output CW/CCW or Step/Dir signals (EEO#.MODE 1 or 2) you will get 4 times this value of pulses per revolution.
Examples
Code
This will set the number of EEO2 lines to 8096.
-->EEO2.LINES 8096
Context
For more information see Output - Encoder Emulation.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 16777215 |
| Default Value | 1024 |
| Data Type | Integer |
| See Also | |
| Stored in Non-Volatile Memory | Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
EEO1.LINES |
4600h |
02h |
Unsigned32 |
- |
- |
Read/Write |
No |
|
EEO2.LINES |
4601h |
02h |
Unsigned32 |
- |
- |
Read/Write |
No |
|
EEO3.LINES |
4603h |
02h |
Unsigned32 |
- |
- |
Read/Write |
No |
|
EEO4.LINES |
4606h |
02h |
Unsigned32 |
- |
- |
Read/Write |
No |
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
EEO1.LINES |
32005 |
7D05 |
Unsigned32 |
Read/Write |
- |
|
EEO2.LINES |
32006 |
7D06 |
Unsigned32 |
Read/Write |
- |
|
EEO3.LINES |
32007 |
7D07 |
Unsigned32 |
Read/Write |
- |
|
EEO4.LINES |
32008 |
7D08 |
Unsigned32 |
Read/Write |
- |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
EEO1.LINES |
32005 |
Unsigned32 |
Read/Write |
- |
|
EEO2.LINES |
32006 |
Unsigned32 |
Read/Write |
- |
|
EEO3.LINES |
32007 |
Unsigned32 |
Read/Write |
- |
|
EEO4.LINES |
32008 |
Unsigned32 |
Read/Write |
- |